Fields that describe the connection to a SQL connection
![]() |
CimSQLTableConnection
Fields that describe the connection to a SQL connection
|
Name | Description | Data Type |
---|---|---|
Table_id | Table id on which connection is updated. | string |
SQLConnection | Fields that describe the connection to a SQL connection | CimSQLConnection |
SQLConnection\ConnectionType | CimSQLConnectionType | |
SQLConnection\ODBCDataSource | ODBC Data connection. | string |
SQLConnection\UserID | User who will connect to the selected database driver. A database user name is required if you are connecting to a SQL Server. | string |
SQLConnection\Passsword | Password needed to connect to the selected database driver. A password is required if you are connecting to a SQL Server. | string |
SQLConnection\ReconnectWaitPeriod | The amount of time that the Database Logger waits between reconnect attempts when the connection to the database is lost. | integer |
SQLConnection\ReconnectWaitUnit | defines units for time values | CimTimeUnitEnum |
SQLConnection\EnableStoreAndForward | Choose enable store and forward to enable the ALARM_LOG table perform store and forward options. | boolean |
SQLConnection\MaxNumberOfStoredRecord | To select the number of records the Database Logger will store when its connection to the database is down. Enter a number between 1 and 4294967285. 0 indicates no limit. | number |